:MEASure:TDEQ:MRUN:THRee
Command Syntax
:MEASure:TDEQ:MRUN:THRee <number of threes>
<number of threes> is an integer.
Query Syntax
:MEASure:TDEQ:MRUN:THRee?
Description
Enters the minimum number of consecutive PAM4 level three UIs that can be used for the OMA/ER definition when measuring TDECQ. The setting can range from 5 to 1024 with the default number of 7. Use the :MEASure:TDEQ:MRUN:ZERO command to specify the minimum number of consecutive PAM4 level zero UIs. If the runs are shorter, the measurement is marked a questionable (a "?" character annotates the measurement's results) and the :MEASure:EYE:TDEQ:STATus? query returns QUES.
This command is equivalent to the Minimum Three Level Run setting which is located in the TDECQ Reference Equalizer Setup dialog's TDECQ Measurement tab. To open this dialog, click on the TDECQ operator in the Waveform Signal Processing Setup dialog.
Requires FlexDCA revision A.07.50 and above.