:STATus:REPository:ENABle
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Command Syntax
:STATus:REPository:ENABle <mask>
<mask> is an integer, 0 to 255, representing a mask for the bits in the event register.
Query Syntax
:STATus:REPository:ENABle?
Description
Enters a decimal-weighted value in the Repository enable register that masks the ability to report bits in the repository event register.
Register | Read | Write | Command |
---|---|---|---|
Event | ♦ | :STATus:REPository:EVENt? | |
Enable (mask) | ♦ | ♦ | :STATus:REPository:ENABle |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|---|
Bit Weight |
128 | 64 | 32 | 16 | 8 | 4 | 2 | 1 |
Event Register |
— | — | — | — | — | — | DCON | CONN |
Enable Register |
||||||||
Sets | to Bit 4 of Operation Status Register |
Bit Definitions
- CONN
- A true indicates that an N8844A server is connected.
- DCON
- A true indicates that an N8844A server has been disconnected.
Requires FlexDCA revision A.05.70 and above.