:STATus:REPository:EVENt?
Instrument:
N1010A
DCA-X
DCA-M
Meas. mode:
Scope
Eye
Jitter
TDR
Flex Apps:
FlexDCA
FlexRT
Query Syntax
:STATus:REPository:EVENt?
Description
Reads the Repository event register to determine the status of individual status bits for the state of the connection to a Keysight N8844A data analytics server. The decimal-weighted value of the register is returned. Bit 0 (CONN), is set when a connection is established to an N8844A data analytics server. Bit 1 (DCON) is set when an N8844A connection is disconnected. Reporting of event register bits in the status register system is controlled by the mask loaded into the enable register. All true event bits, that are enabled, are logically AND'ed, which results in setting true bit 4 (RCON) of the Operation Status Register. Use the :REPository subsystem to configure the N8844A connection.
Register | Read | Write | Command |
---|---|---|---|
Event | ♦ | :STATus:REPository:EVENt? | |
Enable (mask) | ♦ | ♦ | :STATus:REPository:ENABle |
Bit | 7 | 6 | 5 | 4 | 3 | 2 | 1 | 0 |
---|---|---|---|---|---|---|---|---|
Bit Weight |
128 | 64 | 32 | 16 | 8 | 4 | 2 | 1 |
Event Register |
— | — | — | — | — | — | DCON | CONN |
Enable Register |
||||||||
Sets | to Bit 4 of Operation Status Register |
Bit Definitions
- CONN
- A true indicates that an N8844A server is connected.
- DCON
- A true indicates that an N8844A server has been disconnected.
Requires FlexDCA revision A.05.70 and above.