:MEASure:AMPLitude:DEFine:SNDRatio:PDELay
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:AMPLitude:DEFine:SNDRatio:PDELay <UIs>
Where <UIs> is an integer between 1 and 50 with a default value of 4.
Query Syntax
:MEASure:AMPLitude:DEFine:SNDRatio:PDELay?
Query Response
<UIs>
Description
For the SNDR measurement (:MEASure:PLEVel:SNDRatio), sets the pulse delay in unit intervals.
Requires FlexDCA revision A.07.90 and above.
Example Command
:MEASure:AMPLitude:DEFine:SNDRatio:PDELay 4