:MEASure:AMPLitude:DEFine:SNDRatio:DEFinition
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:AMPLitude:DEFine:SNDRatio:DEFinition {PMAX | PSIGnal}
Query Syntax
:MEASure:AMPLitude:DEFine:SNDRatio:DEFinition?
Query Response
{PMAX | PSIGnal}
Description
Selects the method used to calculate the amplitude of the signal by the Signal-to-Noise-and-Distortion Ratio (SNDR) measurement.
- PMAX
- The ideal signal model is based on the peak amplitude of the extracted linear pulse response.
- PSIG
- The ideal signal model is based on the peak amplitude of the linear fit on the measured pulse response. This is the default selection.
Requires FlexDCA revision A.07.90 and above.
Example Command
:MEASure:AMPLitude:DEFine:SNDRatio:DEFinition PMAX