:MEASure:AMPLitude:DEFine:SNDRatio:PLENgth
Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter
Command Syntax
:MEASure:AMPLitude:DEFine:SNDRatio:PLENgth <UIs>
Where <UIs> is an integer between 8 and 1000 with a default value of 200.
Query Syntax
:MEASure:AMPLitude:DEFine:SNDRatio:PLENgth?
Query Response
<UIs>
Description
For the SNDR measurement (:MEASure:PLEVel:SNDRatio), sets the pulse length in unit intervals.
Requires FlexDCA revision A.07.90 and above.
Example Command
:MEASure:AMPLitude:DEFine:SNDRatio:PLENgth 200