:MEASure:JITTer:DDJVsbit:BITS?
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:JITTer:DDJSymbol:SYMBols command instead.
Query Syntax
:MEASure:JITTer:DDJVsbit:BITS?
Description
Returns a list of bits for which :DDJVsbit? has returned values. The bits are returned as definite-length block data. Each bit value is a 32-bit integer (4 bytes) returned in LSB (Least Significant Byte) first format. The data block is followed by a linefeed termination character (0A hex).
Requires Jitter Mode license.
Endiannes of Returned Data
To specify the byte order (endiannes) of the binary data, use the :SYSTem:BORDer command. The factory preset setting is little-endian in which the LSB (Least Significant Byte) is sent first. Because an incorrect endianess setting can be frustrating to troubleshoot, if you share your N1000A with other people, it is a good idea to explicitly set the endianess before transferring binary data and to restore FlexDCA's endianess setting upon completion of of your program. Use the following sequence of commands:
endian_setting = :SYSTem:BORDer? :SYSTem:BORDer BENDian … … :WAVeform:XYFormat:FLOat:YDATa? … … :SYSTem:BORDer endian_setting
Be aware that VXI plug-and-play drivers can change the endianess setting. As a result always explicitly set the endianess in your program before transferring any binary data.
Example Command Sequence
:SYSTem:MODE JITTer :MEASure:JITTer:DDJVsbit? :MEASure:JITTer:DDJVsbit:BITS?