:MEASure:JITTer:ESKew:STATus?
Meas. mode:
Jitter
Package License:
L-RND
Waveform type:
PAM4
Waveform record:
MV
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:PEYE:ESKew:STATus command instead.
Query Syntax
:MEASure:JITTer:ESKew:STATus?
Query Response
{CORR | INV | QUES}
CORR- The measurement result is correct.
INV- The measurement result is invalid. A question mark (?) is shown in the displayed results tableinstead of a measurement result.
QUES- The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.
Description
Queries the status of the measurement. Use the :MEASure:JITTer:ESKew:STATus:REASon? child query to determine the reason for a invalid or questionable measurement. Additional information about the failure may be available using the :STATus:DETails? child query.
Requires FlexDCA revision A.05.60 and above.