:MEASure:JITTer:ESKew:STATus:REASon?
Meas. mode:
Jitter
Package License:
L-RND
Waveform type:
PAM4
Waveform record:
MV
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:PEYE:ESKew:STATus:REASon command instead.
Query Syntax
:MEASure:JITTer:ESKew:STATus:REASon?
Query Response
Refer to the table "Possible Common :STATus:REASon? Query Responses".
Description
Returns a string that explains the reason for a failed :JITTer:ESKew measurement. If the measurement was successful, a null string is returned.
Additional information about the failure may be available using the :STATus:DETails? sibling query. Use the :JITTer:ESKew:STATus? parent query to determine if the measurement has failed.
Requires FlexDCA revision A.05.60 and above.