:MEASure:JITTer:ESKew:LOCation?
Meas. mode:
Jitter
Package License:
L-RND
Waveform type:
PAM4
Waveform record:
MV
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:PEYE:ESKew:LOCation command instead.
Query Syntax
:MEASure:JITTer:ESKew:LOCation?
Description
Returns an index for the location of the ESKew measurement results in the active measurement list. Using this information, you can select, clear, or remove measurement results from the displayed results table. If the measurement is not listed in the table, a "−1" is returned.
Requires FlexDCA revision A.05.60 and above.