:MEASure:JITTer:ESKew:SOURce
Meas. mode:
Jitter
Package License:
L-RND
Waveform type:
PAM4
Waveform record:
MV
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:PEYE:ESKew:SOURce command instead.
Command Syntax
:MEASure:JITTer:ESKew:SOURce <source_waveform>
Where <source_waveform> can be one of the following:
CHANnel{1:8}{A|B|C|D}DIFF{1:4}CGMemory{1:8}FUNCtion{1:16}
Query Syntax
:MEASure:JITTer:ESKew:SOURce?
Description
Selects the source waveform on which to perform the measurement.:MEASure:JITTer:ESKew
Requires FlexDCA revision A.05.60 and above.