:MEASure:JITTer:ESKew
Meas. mode:
Jitter
Package License:
L-RND
Waveform type:
PAM4
Waveform record:
MV
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:PEYE:ESKew command instead.
Command Syntax
:MEASure:JITTer:ESKew
Query Syntax
:MEASure:JITTer:ESKew?
Query Response
unknown
Description
Starts Jitter mode's Eye Skew measurement where the skew (seconds or UI) of an eye is measured on a PAM4 signal. Select the eye to be measured using the :EYE child command. To measure the eye skews for all of the eyes on a PAM4 signal, you must send this command once for each eye as there is no command for simultaneously measuring all eye skews.
Requires FlexDCA revision A.05.60 and above.
Common Measurement Child Queries
Common measurement queries. :COUNt?, :LOCation?, :MAXimum?, :MINimum?, :MEAN?, and :SDEViation?.