:MEASure:JITTer:ESKew:STATus:DETails?
Meas. mode:
Jitter
Package License:
L-RND
Waveform type:
PAM4
Waveform record:
MV
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:PEYE:ESKew:STATus:DETails command instead.
Query Syntax
:MEASure:JITTer:ESKew:STATus:DETails?
Description
Returns a string that may provide additional details for a failed :JITTer:ESKew measurement. If the measurement was successful, a null string is returned.
For a basic description of a measurement failure, use the :STATus:REASon? sibling query. Use the :STATus? parent query to determine if the measurement has failed.
Requires FlexDCA revision A.05.60 and above.