:MEASure:JITTer:ESKew:EYE
Meas. mode:
Jitter
Package License:
L-RND
Waveform type:
PAM4
Waveform record:
MV
Command:
Deprecated
Deprecated command. For FlexDCA revision A.05.60 and above, use the :MEASure:PEYE:ESKew:EYE command instead.
Command Syntax
:MEASure:JITTer:ESKew:EYE {EYE0 | EYE1 | EYE2}
Query Syntax
:MEASure:JITTer:ESKew:EYE?
Description
This command allows you to select an eye on PAM4 signals. For NRZ signals, the 0 eye is automatically selected and cannot be changed. The command selects the PAM4 eye on which to perform the :MEASure:JITTer:ESKew. The query form of the command returns the currently selected eye.
Requires FlexDCA revision A.05.60 and above.