:MEASure:JITTer:OJITter:SJNU
Deprecated command. For FlexDCA revision A.06.00 and above, use the :MEASure:JITTer:OJITter:JNU:SJNU command instead.
Command Syntax
:MEASure:JITTer:OJITter:SJNU {J1U | J2U | J3U | J4U | J5U}
Query Syntax
:MEASure:JITTer:OJITter:SJNU?
Query Response
{J1U | J2U | J3U | J4U | J5U}
Description
For an IEEE 12-Edge Output Jitter measurement, selects an output jitter measurements that are based on a specific probability as listed in the following table.
| Argument | Probability |
|---|---|
| J5U | 10–5 |
| J4U | 10–4 |
| J3U | 10–2 |
| J2U | 10–1 |
| J1U | 10–1 |
To select the waveform's edge (edge category) for the measurement, use the :MEASure:JITTer:OJITter:JNU:ECATegory command. To return the measurement, use the :MEASure:JITTer:OJITter:JNU? query. The measurement result is always for a specified type and edge category.
This command is equivalent to the Select Jnu Type field in the Jitter Measurements tab of the Jitter Mode Measurement Setup dialog. Use the :DISPlay:JITTer:OJITter:ECATegory command to select the type of waveform edge (edge category) on which to construct the displayed Output Jitter Histogram graph.
Requires FlexDCA revision A.05.85 and above.