:MEASure:TDEQ:CER:CSLength

Meas. mode:
Eye
Waveform type:
PAM4
Flex Apps:
FlexDCA

Command Syntax

:MEASure:TDEQ:CER:CSLength <integer>

Where <integer> is a integer between 1 and 1024.

Query Syntax

:MEASure:TDEQ:CER:CSLength?

Query Response

<integer>

Description

Sets the Codeword Length in bits. The default value is 64 bits. The minimum value is 1 bit. The maximum value is 1024 bits. The Codeword Length is applied to CER TDECQ (:MEASure:EYE:CTDecq) and CER Noise Margin (rms) (:MEASure:EYE:CNMargin) measurements.

Requires FlexDCA revision A.08.30 and above.

Example Command

:MEASure:TDEQ:CER:CSLength 128