:MEASure:TDEQ:CER:PRESets:SELections?

Meas. mode:
Eye
Waveform type:
PAM4
Flex Apps:
FlexDCA

Query Syntax

:MEASure:TDEQ:CER:PRESets:SELections?

Query Response

"preset name, preset name, preset name, …"

Description

Returns a string which is a comma-separated list of all saved presets for the CER TDECQ measurement (:MEASure:EYE:CTDecq) and the CER Noise Margin (rms) measurement (:MEASure:EYE:CNMargin). Use the :MEASure:TDEQ:CER:PRESets parent command to load a preset.

Requires FlexDCA revision A.08.30 and above.

Example Command

:MEASure:TDEQ:CER:PRESets:SELections?