:MEASure:TDEQ:CER:NCORrectable
Meas. mode:
Eye
Waveform type:
PAM4
Flex Apps:
FlexDCA
Command Syntax
:MEASure:TDEQ:CER:NCORrectable <integer>
Where <integer> is an integer from 0 to 64.
Query Syntax
:MEASure:TDEQ:CER:NCORrectable?
Query Response
<integer>
Description
Sets the number of Correctable Symbols. The number of correctable symbols can be any integer from 0 to 64. The default value is 3. The Correctable Symbols is applied to CER TDECQ (:MEASure:EYE:CTDecq) and CER Noise Margin (rms) (:MEASure:EYE:CNMargin) measurements.
Requires FlexDCA revision A.08.30 and above.
Example Command
:MEASure:TDEQ:CER:NCORrectable 32