:MEASure:TDEQ:CER:SPFSymbol

Meas. mode:
Eye
Waveform type:
PAM4
Flex Apps:
FlexDCA

Command Syntax

:MEASure:TDEQ:CER:SPFSymbol <integer>

Where <integer> is an integer between 1 and 16.

Query Syntax

:MEASure:TDEQ:CER:SPFSymbol?

Query Response

<integer>

Description

Sets the number of Signal Symbols Per Codeword Symbol. The value can be an integer between 1 and 16. The default value is 1. Signal Symbols Per Codeword Symbol is applied to CER TDECQ (:MEASure:EYE:CTDecq) and CER Noise Margin (rms) (:MEASure:EYE:CNMargin) measurements.

Requires FlexDCA revision A.08.30 and above.

Example Command

:MEASure:TDEQ:CER:SPFSymbol 5