:MEASure:TDEQ:CER:TARGet
Meas. mode:
Eye
Waveform type:
PAM4
Flex Apps:
FlexDCA
Command Syntax
:MEASure:TDEQ:CER:TARGet <double>
Where <double>. For example, 0.000100.
Query Syntax
:MEASure:TDEQ:CER:TARGet?
Query Response
<double>
Description
Sets the Target CER (Codeword Error Ratio) for the CER TDECQ (:MEASure:EYE:CTDecq) and CER Noise Margin (rms) (:MEASure:EYE:CNMargin) measurements. By default, the Target CER tracks the Target SER (Symbol Error Ratio). To set the Target CER, you must first disable tracking with the :MEASure:TDEQ:CER:TSER command.
The minimum value of Target CER is 10–15, the maximum value is 100E–3, and the default value is 100E–6.
Requires FlexDCA revision A.08.30 and above.
Example Command
:MEASure:TDEQ:CER:TARGet