:MEASure:TDEQ:CER:INTerleaving

Meas. mode:
Eye
Waveform type:
PAM4
Flex Apps:
FlexDCA

Command Syntax

:MEASure:TDEQ:CER:INTerleaving <integer>

Where <integer> is an integer from 1 to 64. For example, 8.

Query Syntax

:MEASure:TDEQ:CER:INTerleaving?

Query Response

<integer>

Description

Sets the Interleaving Count. The count can be any integer from 1 to 64. The default value is 8. The Interleaving Count is applied to CER TDECQ (:MEASure:EYE:CTDecq) and CER Noise Margin (rms) (:MEASure:EYE:CNMargin) measurements.

Requires FlexDCA revision A.08.30 and above.

Example Command

:MEASure:TDEQ:CER:INTerleaving 16