:MEASure:TDEQ:CER:TSER

Meas. mode:
Eye
Waveform type:
PAM4
Flex Apps:
FlexDCA

Command Syntax

:MEASure:TDEQ:CER:TSER {ON | OFF}

Query Syntax

:MEASure:TDEQ:CER:TSER?

Query Response

{0 | 1}

Description

The TSER (track SER) command turns on or off the ability of the Target CER (Codeword Error Ratio) to track the Target SER (Symbol Error Ratio). By default, tracking is turned on. When tracking is turned off, you can set the Target CER using the :MEASure:TDEQ:CER:TARGet command. Target CER is applied to CER TDECQ (:MEASure:EYE:CTDecq) and CER Noise Margin (rms) (:MEASure:EYE:CNMargin) measurements.

Requires FlexDCA revision A.08.30 and above.

Example Command

:MEASure:TDEQ:CER:TSER OFF