:SPRocess:TEQualizer:FIBer:ENABle

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical

Command Syntax

:SPRocessN:TEQualizer:FIBer:ENABle {ON | OFF}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:TEQualizer:FIBer:ENABle?

Description

Turns on a modal dispersion filter for the TDECQ Equalizer operator. Use the :SPRocess:TEQualizer:FIBer:BANDwidth command to enter the bandwidth of the filter.

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:FIBer:ENABle command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:FIBer:ENABle

Requires FlexDCA revision A.06.90 and above.