:SPRocess:TEQualizer:MNPRecursors

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical

Command Syntax

:SPRocessN:TEQualizer:MNPRecursors <integer>

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Where <integer> is an integer.

Query Syntax

:SPRocessN:TEQualizer:MNPRecursors?

Query Response

<integer>

Description

When the TDECQ operator is set to automatically configure the precursors (:SPRocess:TEQualizer:NPRecursors:AUTO), this command allows you to set or query the limit for maximum number of precursors. This is equivalent to setting the Max Precursors setting in the Taps tab of the TDECQ Reference Equalizer Setup dialog.

The default value is 3. The minimum value is 0. The maximum value is 4.

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:MNPRecursors command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:MNPRecursors

Requires FlexDCA revision A.05.80 and above.