:SPRocess:TEQualizer:TAPS:COUNt

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical

Command Syntax

:SPRocessN:TEQualizer:TAPS:COUNt <count>

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Where <count> is a integer of the number of taps.

Query Syntax

:SPRocessN:TEQualizer:TAPS:COUNt?

Description

Specifies the number of taps for the TDECQ Equalizer operator. Increasing the number of taps in your model increases the fidelity of the filter's frequency response as compared to an ideal response. To enter the precursors, use the :SPRocess:TEQualizer:NPRecursors command. Before you can use these commands, turn on the automatic determination of tap values (:SPRocess:TEQualizer:TAPS:AUTo ON).

To manually enter tap values, first disable automatic tap configuration (:SPRocess:TEQualizer:TAPS:AUTo OFF), then use the :SPRocess:TEQualizer:TAPS command.

Use of an *OPC? query to pause program execution while waiting for this command to execute.

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:TAPS:COUNt command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:TAPS:COUNt

Requires FlexDCA revision A.05.60 and above.