:SPRocess:TEQualizer:TAPS:IOPTimize

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical

Command Syntax

:SPRocessN:TEQualizer:TAPS:IOPTimize {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:TEQualizer:TAPS:IOPTimize?

Description

Turns on Iterative Optimization which allows you to define seed taps for the TDECQ operator's Feed Forward equalizer using the :SPRocess:TEQualizer:TAPS:SEED command. Use the :SPRocess:TEQualizer:TAPS:SEED:COPy command to use the current tap values as seed taps for iterative optimization. Once you have configured you taps, use the :SPRocess:TEQualizer:TAPS:SEED:ENABle command to enable the seed taps.

Turning Iterative Optimization on disables the use of the TDECQ operator's Decision Feedback Equalizer.

Always follow this command with a *OPC? query to halt program execution until the command completes.

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:TAPS:IOPTimize command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:TAPS:IOPTimize

Requires FlexDCA revision A.05.70 and above.