:SPRocess:TEQualizer:TAPS:RECalculate

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical

Command Syntax

:SPRocessN:TEQualizer:TAPS:RECalculate

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Description

Initiates a re-calculation of the tap values for the TDECQ Equalizer operator. Do not follow this command with an *OPC? command. Automatic tap configuration must first be enabled (:SPRocess:TEQualizer:TAPS:AUTo ON).

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:TAPS:RECalculate command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:TAPS:RECalculate

Requires FlexDCA revision A.05.60 and above.