:SPRocess:TEQualizer:TAPS

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical

Command Syntax

:SPRocessN:TEQualizer:TAPS <tap_value>,<tap_value>, …

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:TEQualizer:TAPS?

Description

Enters a list of tap values for the TDECQ Equalizer operator. Increasing the number of taps in your model increases the fidelity of the filter's frequency response as compared to an ideal response. To use this command, automatic tap configuration must be turned off using the :SPRocess:TEQualizer:TAPS:AUTo command.

The query form of the command returns a list of the current tap values.

Use of an *OPC? query to pause program execution while waiting for this command to execute.

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:TAPS command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:TAPS

Requires FlexDCA revision A.05.60 and above.