:SPRocess:TEQualizer:TAPS:SEED:ENABle

Instrument:
N1000A
N109x
Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical
Package License:
L-RND

Command Syntax

:SPRocessN:TEQualizer:TAPS:SEED:ENABle {ON | OFF | 1 | 0}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:TEQualizer:TAPS:SEED:ENABle?

Description

When Iterative Optimization is turned on for the TDECQ equalizer, enables the application of the seed taps that are defined using the :SPRocess:TEQualizer:TAPS:SEED and the :SPRocess:TEQualizer:TAPS:SEED:COPy commands. To turn on Iterative Optimization, use the :SPRocess:TEQualizer:TAPS:IOPTimize command

Always follow this command with a *OPC? query to halt program execution until the command completes.

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:TAPS:SEED:ENABle command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:TAPS:SEED:ENABle

Requires FlexDCA revision A.05.70 and above.