:SPRocess:TEQualizer:PRESets:SELections?
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical
Query Syntax
:SPRocess:TEQualizer:PRESets:SELections?
Query Response
"preset name, preset name, preset name, …"
Description
Returns a string which is a comma-separated list of all saved presets for the TDECQ Equalizer operator. Use the PRESet command to load one of these presets.
TDECQ Equalizer Presets
- IEEE 802.3dj Draft 2.0
- IEEE 802.3bs Amended
- IEEE 802.3bs
- IEEE 802.3cd
- IEEE 802.3db SR SECQ
- IEEE 802.3db SR (844-863 nm)
- IEEE 802.3db VR (842-948 nm)
- IEEE 802.3db VR (842-918 nm)
- IEEE 802.3db VR (842-888 nm)
- IEEE 802.3db VR (842-868 nm)
- Fiber Channel PI - 7 Rev 0.13
- TDEC ITU 50G PON OLT
- TDEC ITU 50G PON ONU
For Reference Rx operator, what function do I send this command to?
If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:PRESets:SELections command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:
:SPRocess2:TEQualizer:PRESets:SELections
Requires FlexDCA revision A.05.60 and above.