:SPRocess:TEQualizer:NPRecursors:AUTO

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical

Command Syntax

:SPRocessN:TEQualizer:NPRecursors:AUTO {ON | OFF}

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:TEQualizer:NPRecursors:AUTO?

Query Response

 {ON | OFF | 1 | 0}

Description

Sets automatic configuration of the TDECQ operator precursors on or off:

ON
Automatic configuration is on, which is the default setting. Use the :SPRocess:TEQualizer:MNPRecursors command to set or query the maximum number of precursors allowed.
OFF
Automatic configuration is off. When setting automatic configuration off, follow the command with the *OPC? query. Use the :SPRocess:TEQualizer:NPRecursors parent command to manually set or query the number of precursors for the operator.

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:NPRecursors:AUTO command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:NPRecursors:AUTO

Requires FlexDCA revision A.05.80 and above.