:SPRocess:TEQualizer:NPRecursors

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical

Command Syntax

:SPRocessN:TEQualizer:NPRecursors <number>

<number> is an integer.

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Query Syntax

:SPRocessN:TEQualizer:NPRecursors?

Description

For the TDECQ operator, turns on and off automatic generation of precursors for the operator's Feed Forward Equalizer and Decision Feedback Equalizer. The default setting is 0. The query form of the command returns the current setting.

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:NPRecursors command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:NPRecursors

Requires FlexDCA revision A.05.60 and above.