:SPRocess:TEQualizer:TAPS:NORMalize

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical

Command Syntax

:SPRocessN:TEQualizer:TAPS:NORMalize

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Description

Automatically adjusts the tap values of the TDECQ Equalizer operator for a maximum equalizer gain of 0 dB (unity). The relative contributions of the tap values are maintained. Automatic tap configuration must be disabled (:SPRocess:TEQualizer:TAPS:AUTo OFF).

Use of an *OPC? query to pause program execution while waiting for this command to execute.

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:TAPS:NORMalize command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:TAPS:NORMalize

Requires FlexDCA revision A.05.60 and above.