:SPRocess:TEQualizer:TAPS:LIMits:MAIN:MAX

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical

Command Syntax

:SPRocessN:TEQualizer:TAPS:LIMits:MAIN:MAX "tap_value"

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Where "tap_value" is a double. For example, 0.10.

Query Syntax

:SPRocessN:TEQualizer:TAPS:LIMits:MAIN:MAX?

Description

Enters a maximum value of the Main tap for the TDECQ Equalizer operator. To apply your tap limits, use the :SPRocess:TEQualizer:TAPS:LIMits:STATe command.

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:TAPS:LIMits:MAIN:MAX command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:TAPS:LIMits:MAIN:MAX

The Linear Feedforward Equalizer operator is provided with the N1010A-201 Advanced Waveform Analysis license.

Requires FlexDCA revision A.07.80 and above.