:SPRocess:TEQualizer:TAPS:SEED:COPy

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical

Command Syntax

:SPRocessN:TEQualizer:TAPS:SEED:COPy

Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.

Description

When Iterative Optimization is turned on for the TDECQ equalizer, copies the current automatically calculated tap values to use as the seed taps. To turn on Iterative Optimization, use the :SPRocess:TEQualizer:TAPS:IOPTimize command. Once you have configured you taps, use the :SPRocess:TEQualizer:TAPS:SEED:ENABle command to enable the seed taps.

Always follow this command with a *OPC? query to halt program execution until the command completes.

For Reference Rx operator, what function do I send this command to?

If the TDECQ equalizer is a secondary function to the Reference Rx operator, address the :SPRocess:TEQualizer:TAPS:SEED:COPy command to the Reference Rx function as identified in the following Reference Rx Setup dialog's operator diagram. In the following figure, this would be Function 2 and the command would be:

:SPRocess2:TEQualizer:TAPS:SEED:COPy

Requires FlexDCA revision A.05.70 and above.