Ceq Noise Gain

Flex Apps:
FlexDCA
FlexRT
Meas. mode:
Eye
Waveform type:
PAM4
NRZ

The Eye mode PAM Ceq noise gain measurement measures the noise gain introduced by the following FlexDCA Waveform Signal Processing operators. To perform this measurement, one of the following operators must be installed.

Although the Ceq measurement is defined by the standard for TDECQ measurements, it can be used with any of the operators that are listed above. Ceq is expressed as:

This measurement does not support PAM6 or PAM8 waveforms.