:MEASure:JITTer:DEFine:LEVel:PERCent:EYE

Flex Apps:
FlexDCA
Meas. mode:
Jitter
Waveform type:
NRZ
Meas. panel:
Jitter

Command Syntax

:MEASure:JITTer:DEFine:LEVel:PERCent:EYE{N} <percent>

{N} is 0 for an NRZ signal and 0, 1, or 2 for a PAM4 signal.

<percent> is a double.

Query Syntax

:MEASure:JITTer:DEFine:LEVel:PERCent:EYE{N}?

Description

For the specified eye, sets the jitter sampling level as a percent of Unit Interval (UI). For NRZ signals, this is the value for the single eye. For PAM4 signals, you can individually specify the percentage that is used for each of the three eyes. The value must be between 30% and 70%. For NRZ signals, the default value is 50.00%. For PAM4 signals, the default values are 16.67% (Eye 0), 50.00% (Eye 1), and 83.33% (Eye 2).

To enter percent, the :MEASure:JITTer:DEFine:LEVel:TYPe command must be set to PERCent.

Requires FlexDCA revision A.05.60 and above. This command replaces deprecated command :MEASure:JITTer:DEFine:LEVel:PERCent.