:MEASure:EYE:CNMargin:STATus?

Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM4

Query Syntax

:MEASure:EYE:CNMargin:STATus?

Query Response

{CORR | INV | QUES}

CORR
The measurement result is correct.
INV
The measurement result is invalid. A question mark (?) is shown in the displayed results table instead of a measurement result.
QUES
The measurement result is questionable. A question mark (?) is shown in the displayed results table next to the measurement result.

Description

Queries the status of the :MEASure:EYE:CNMargin? measurement. Use the :MEASure:EYE:CNMargin:STATus:REASon? query to determine the reason for a invalid or questionable measurement. Use the :MEASure:EYE:CNMargin:STATus:DETails? query to determine additional details for a failure.

Requires FlexDCA revision A.08.30 and above.