:SPRocess:TPARameter:THReshold?
Flex Apps:
FlexDCA
Meas. mode:
Eye
Waveform type:
PAM
NRZ
Optical
Electrical
Query Syntax
:SPRocessN:TPARameter:THReshold? EYE{0:7}
Where N identifies one of up to 64 possible operators {1:64} that can be defined as part of a math function. The operators are numbered in the order that they were originally added to the function.
Query Response
threshold
Where threshold is a double. If the threshold value is undefined, the string "9.91E+37 (NaN)" is returned.
Description
For TDECQ measurements on the TDECQ operator's output waveform, returns the threshold level in Watts or volts for the selected eye. In the following screen capture, this parameter is identified as 84 μW for Eye 0, 250 μW for Eye 1, and 416 μW for Eye 2.
Requires FlexDCA revision A.08.30 and above.