:CALibrate:MODule:SLOT:STATus?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.01.70 and above, use the :CALibrate:SLOT:STATus? command.
Query Syntax
:CALibrate:MODule:{SLOT{1:8} | LMODule | RMODule}:STATus?
Description
Queries the calibration status of a module. 86108A modules are identified as being installed in :SLOT1. One of the following response strings are returned:
- "CALIBRATED"
- The module does not require a calibration.
- "UNCALIBRATED"
- The module requires a calibration.
Use the child queries listed in the following table to return details about the current calibration.
| Status Sring | Child Query to Send |
|---|---|
| Time of last calibration, Time change since last calibration, and Ttemperature change since last calibration |
:DETails?
|
| Change in temperature | :TEMPerature?
|
| Change in Time | :TIME?
|