:CALibrate:CRECovery:SLOT:STARt

Command:
Deprecated
Flex Apps:
FlexDCA

Deprecated command. For FlexDCA revision A.01.70 and above, use the :CALibrate:SLOT:CRECovery command.

Command Syntax

:CALibrate:CRECovery:{SLOT{N} | LMODule | RMODule}:STARt

{N} identifies a specific module by slot and must be selected from {1:8}. For a module that occupies multiple slots, use the module's left-most slot number to identify the module. For two-slot modules, the slot number would be 1 or 3. For four-slot modules like the 86108B, the slot number would be 1.

Description

Starts a calibration on a clock recovery module. The *OPC? query should be used to detect when a portion of the calibration has completed. Use the CONTinue command to dismiss dialogs that are displayed during a calibration. SLOT1 identifies a module that is installed in the left module bay. SLOT3 identifies a module that is installed in the right module bay.

Example Command Sequence

:CALibrate:CRECovery:SLOT1:STARt
*OPC?
…  //  Your code to synchronize execution timing.
:CALibrate:CONTinue
*OPC?
…  //  Your code to synchronize execution timing.
:CALibrate:CONTinue