:CALibrate:VERTical:SLOT:STATus:TIME?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.01.70 and above, use the :CALibrate:SLOT:VERTical:STATus:TIME? command.
Query Syntax
:CALibrate:VERTical:{SLOT{1:8} | LMODule | RMODule}:STATus:TIME?
Description
Queries the time of the last electrical or optical vertical channel calibration. Use the :CALibrate:VERTical:SLOT<N>:STARt command to start a vertical calibration.
Example Returned Status String
"08/18/2011 08:14:02"
Example Command
:CALibrate:VERTical:SLOT3:STATus:TIME?