:CALibrate:MODule:SLOT:STARt

Command:
Deprecated
Flex Apps:
FlexDCA

Deprecated command. For FlexDCA revision A.01.70 and above, use the :CALibrate:SLOT:STARt command.

Command Syntax

:CALibrate:MODule:{SLOT{1:8} | LMODule | RMODule}:STARt

Description

Starts the vertical calibration or the precision timebase and clock recovery calibration. The *OPC? query should be used to detect when a portion of the calibration has completed. Use the CONTinue command to dismiss dialogs that are displayed during a calibration. Notice that SLOT1 identifies the module.

Example Command Sequence

:CALibrate:MODule:SLOT1:STARt
*OPC?
…  //  Your code to synchronize execution timing.
:CALibrate:CONTinue