:CALibrate:VERTical:SLOT:STARt

Command:
Deprecated
Flex Apps:
FlexDCA

Deprecated command. For FlexDCA revision A.01.70 and above, use the :CALibrate:SLOT:VERTical command.

Command Syntax

:CALibrate:VERTical:{SLOT{1:8} | LMODule | RMODule}:STARt

Description

Starts an electrical or optical channel vertical calibration. For example, use this command for 86112A, 86105C, and 86107A modules. The *OPC? query should be used to detect when a portion of the calibration has completed. Use the CONTinue command to dismiss dialogs that are displayed during a calibration. SLOT1 identifies a module that is installed in the left module bay. SLOT3 identifies a module that is installed in the right module bay. If a vertical calibration is performed on a TDR module, the :CALibrate:LRESistance command is used to enter the load resistance.

Example Command Sequence

:CALibrate:VERTical:SLOT3:STARt
*OPC?
…  //  Your code to synchronize execution timing.
:CALibrate:CONTinue
*OPC?
…  //  Your code to synchronize execution timing.
:CALibrate:CONTinue
*OPC?
…  //  Your code to synchronize execution timing.
:CALibrate:CONTinue