:CALibrate:FRAMe:STATus:TIME?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.03.00 and above, use the :CALibrate:FRAMe:TIMebase:STATus:TIME? command.
Query Syntax
:CALibrate:FRAMe:STATus:TIME?
Description
Queries the date and time when the last N1000A frame calibration was performed. If a calibration has not yet been performed, an empty string is returned.
Requires FlexDCA revision A.02.00 and above.
Example Returned Status String
"10/20/2011 15:24:48"