:CALibrate:CRECovery:SLOT:STATus?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.01.70 and above, use the :CALibrate:SLOT:CRECovery:STATus? command.
Query Syntax
:CALibrate:CRECovery:{SLOT{N} | LMODule | RMODule}:STATus?
{N} identifies a specific module by slot and must be selected from {1:8}. For a module that occupies multiple slots, use the module's left-most slot number to identify the module. For two-slot modules, the slot number would be 1 or 3. For four-slot modules like the 86108B, the slot number would be 1.
Description
Queries the calibration status of a clock recovery module. Modules are identified as being installed in :SLOT1 or :SLOT3. One of the following response strings are returned:
- "CALIBRATED"
- The module does not require a calibration.
- "UNCALIBRATED"
- The module requires a calibration.
Use the child queries listed in the following table to return details about the current calibration.
| Status Sring | Child Query to Send |
|---|---|
| Time of last calibration, Time change since last calibration, and Ttemperature change since last calibration |
:DETails?
|
| Change in temperature | :DTEMperature?
|
| Change in Time | :TIME?
|