:CALibrate:MODule:SLOT:STATus:TIME?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.01.70 and above, use the :CALibrate:SLOT:STATus:TIME? command.
Query Syntax
:CALibrate:MODule:{SLOT{1:8} | LMODule | RMODule}:STATus:TIME?
Description
Queries the time when the last vertical calibration or precision timebase/clock recovery calibration was performed. A Use the :CALibrate:MODule:SLOT1:STARt command to start a calibration.
Example Returned Status String
"08/18/2011 08:14:02"
Example Command
:CALibrate:MODule:SLOT1:STATus:TIME?