:CALibrate:MODule:SLOT:STATus:DETails?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.01.70 and above, use the :CALibrate:SLOT:STATus:DETails? command.
Query Syntax
:CALibrate:MODule:{SLOT{1:8} | LMODule | RMODule}:STATus:DETails?
Description
Queries a string that lists the following calibration status information for the module. Modules are identified as being installed in :SLOT1.
- Any need for vertical calibration, precision timebase calibration, or clock recovery calibration
- Time of last calibration
- Time change since the last calibration
- Temperature change since last calibration
Example Returned Status String
"Requires Vertical Calibration.,Requires Precision Timebase and Clock Recovery Calibration., Time of last Calibration: 08/03/2011 13:19:02,Elapsed Calibration Time: 355 hours 15 minutes,Temperature Change: 11.4°C"
Example Command Sequence
:CALibrate:MODule:SLOT1:STATus:DETails?