:CALibrate:FRAMe:STATus:DETails?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.03.00 and above, use the :CALibrate:FRAMe:TIMebase:STATus:DETails? command.
Query Syntax
:CALibrate:FRAMe:STATus:DETails?
Description
Queries a string of status details for the N1000A frame.
Requires FlexDCA revision A.02.00 and above.
Example Returned Status
"The temperature has changed by more than 5.00 C.,Time of last Calibration: 10/20/2011 15:24:48,Elapsed Calibration Time: 362 days,Temperature Change: 7.35 C"