:CALibrate:FRAMe:STATus:DTEMperature?
Command:
Deprecated
Flex Apps:
FlexDCA
Deprecated command. For FlexDCA revision A.03.00 and above, use the :CALibrate:FRAMe:TIMebase:STATus:DTEMperature? command.
Query Syntax
:CALibrate:FRAMe:STATus:DTEMperature?
Description
Queries the change in the N1000A frame's temperature from the time when the last frame calibration was performed. If a calibration has not yet been performed, a value of NaA (9.91E+37) is returned. A calibration should be performed if the change in N1000A temperature exceeds ±5°C.
Requires FlexDCA revision A.02.00 and above.
Example Returned Status
7.110000000E+00